Other Parts Discussed in Thread: MSP430F5529, , ENERGIA, MSP-EXP430F5529LP, PGA460, BOOSTXL-PGA460
Hello all,
I have the following setup: I'm using the MSP430F5529 LaunchPad as Master Controller and want to connect the PGA460PSM as slave to it. So far I've connected the devices according the "PGA460PSM-EVM Users Guide" (slau817) in USART mode (according chapter 2.2.2.1).
For my understanding the EVM GUI is conceived for the BOOSTXL460 package, hence after connecting the LP to the PC and running the GUI, I get the dialog to upload the boostxl460 firmware on the LP. Is there a specific firmware for the PGA460PSM module or what do I need to do in order to configure my PGA460PSM inside the EVM GUI?
I want to fintune the PGA since I already got the sample codes via Energia running, but the results were not satisfying, e.g. for the "GetDistance" sample.
Thank you in advance for your help!