Part Number: DRV425EVM
Other Parts Discussed in Thread: DRV425
We are evaluating the DRV425 fluxgate IC using the DRV425EVM evaluation module, and are seeing a substantial amount of ringing on VOUT. Please see the attached (YELLOW is Vout, Blue is Vref). The only loading is the scope probe.
It seems like there is a periodic disturbance to the diff amp at ~500kHz (the chopper clock, perhaps?), which excites ringing in the 2-3MHz range, which is in line with the diff amp bandwidth.
I assume this behavior is not expected. Any insight here is greatly appreciated!