Other Parts Discussed in Thread: IWR6843, , IWR1443, IWR6843ISK
I am developing a new project based on IWR6843, I taking the swrc356a (IWR6843ISK-ODS rev.c) as a reference. This design is working at 60GHZ, the PCB material of TI EVM is Ro3003/5mil. I have designed a project based on IWR1443, which worked at 77GHZ, the PCB material of TI EVM is Ro4350b/4mil.
In general, the performance of Ro3003 is better than Ro4350b. so I wonder why does IWR6843ISK-ODS uses the better material but works at a lower frequency? Are there any special considerations here?
I have communicated with lots of PCB factory, they said the Ro3003 was not a regular material, if they are required to use Ro3003, they must prepare it for a very long time, but the Ro4350b is regular material for RF PCB.
So I want to use Ro4350b to produce my new IWR6843 based design. I wonder if the dimension of antenna in current EVM IWR6843ISK-ODS rev.c applies to R04350b directly? If no, how do I re-design the dimension of antenna? Are there some guidelines available?