Hi Team,
we currently have a project, use LM63 to control Fan speed.
but when setting the PWM frequency, it is found that if the 4D value is set to 0x07, the duty cycle 4C value( 0~14) is set to 0x14~0x10 will be 100%, and it will not become 64.2% until it is set to 0x09.
we use i2c (100kHz) to write the value, and the read value is also correct, but PWM signal output have a problem. could you help confirm or any suggestion for us.
i2cset -f -y 0 0x4c 0x4D 0x07
i2cset -f -y 0 0x4c 0x4c 0x10 "