This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: MMWAVE Studio RF Power up fails

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: MMWCAS-DSP-EVM,

Hello,

I am using an MMWCAS-RF-EVM (Rev - D) with an MMWCAS-DSP-EVM and following the mmwaveStudio studio user guide section 7.3 to attempt to configure the cascade radar. All steps to configure 'RadarDevice1' up to 'Click RF Power-Up' appear to complete successfully. However, once I click 'RF Power-Up' the following appears in the output log:

[14:27:06]  [RadarAPI]: Device Restart failed
[14:27:06]  [RadarAPI]: ar1.RfEnable_mult(1)
[14:27:06]  Status: Failed, Error Type: INVALID INPUT
[14:27:10]  BSS Power Up async event was not received!

I am using mmwaveStudio version 3.0.0.14 with the mmwave DFP version 2.2.2.1 and the metaImage provided by the DFP at mmwave_dfp_02_02_02_01\firmware\xwr22xx_metaImage.bin.

Any advice would be appreciated.

Full output log is below:

GM: Constructor
GM: Tue Sep 01 13:53:43 2020
RSTD.Transmit("/Settings")
[13:53:43]  
[13:53:43]  ### Running Startup script: "C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\Scripts\Startup.lua" ###
[13:53:43]  RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[13:53:43]  RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[13:53:43]  Scripter ignored: Attempt to UnBuild() again or before Build.
[13:53:43]  RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_03_00_00_14\\mmWaveStudio\\Clients\\\\LabClient.dll")
[13:53:43]  RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[13:53:43]  RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[13:53:43]  RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[13:53:43]  RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[13:53:43]  RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[13:53:43]  RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_03_00_00_14\\mmWaveStudio\\RunTime\\SAL.dll")
[13:53:43]  RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[13:53:43]  RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[13:53:43]  RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[13:53:43]  RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[13:53:43]  RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[13:53:43]  RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[13:53:43]  RSTD.Transmit("/")
[13:53:44]  RSTD.Build()
[13:53:44]  RSTD.Transmit("/")
[13:53:44]  RSTD.AL_Build()
[13:53:44]  RSTD.AL_LoadXml()
[13:53:44]  RSTD.Transmit("/")
[13:53:44]  RSTD.AL_Init()
[13:53:44]  RSTD.Clients_Build()
[13:53:44]  GM: Init
[13:53:44]  GM: Loaded 'C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\Clients\\LabClient.dll'
[13:53:44]  GM: 1 Guest (s) init
[13:53:44]  GM: 1 Module(s) init
[13:53:44]  GM: 2 Tab   (s) init
[13:53:44]  RSTD.Client_LoadXml()
[13:53:44]  [RadarAPI]: ar1.selectRadarMode(0)
[13:53:44]  [RadarAPI]: Status: Passed
[13:53:44]  Matlab Runtime Engine is installed
[13:53:44]  [RadarAPI]: Starting Matlab Engine..
[13:53:48]  [RadarAPI]: Matlab Engine Started!
[13:53:50]  [RadarAPI]: ar1.selectCascadeMode(0)
[13:53:50]  [RadarAPI]: Status: Passed
[13:53:50]  TESTING = false
[13:53:50]  RstdNet: Port 2777: Listening..
[13:53:50]  
[13:53:50]  ***Script completed successfully.***
[13:57:30]  [RadarAPI]: ar1.selectRadarMode(1)
[13:57:30]  [RadarAPI]: ar1.selectCascadeMode(1)
[13:57:30]  [RadarAPI]: Status: Passed
[13:57:30]  [RadarAPI]: Status: Passed
[13:57:31]  [RadarAPI]: ar1.SelectCaptureDevice("TDA2XX")
[13:57:31]  [RadarAPI]: Status: Passed
[13:57:33]  [RadarAPI]: TDAStatusCallback Event Registered
[13:57:33]  [RadarAPI]: registerTDAStatusCallback Status: Passed
[13:57:33]  [RadarAPI]: ar1.ConnectTDA("192.168.20.25", 5001, 15)
[13:57:33]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[13:57:33]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[13:57:34]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_VERSION_INFO Async event recieved() with status 0. TDA Version : REL_VISION_SDK_03_07_01_00 Aug  5 2019 15:04:45[13:57:34]  [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[13:57:35]  [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[13:57:35]  [RadarAPI]: ConnectTDACaptureCard Status: Passed
[13:57:35]  TDA Capture Card Status : CONNECTED!
[13:58:27]  [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[13:58:27]  [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0 
[13:58:28]  [RadarAPI]: ar1.FullReset(1)
[13:58:28]  [RadarAPI]: Status: Passed
[13:58:28]  [RadarAPI]: ar1.SOPControl_mult(1,4)
[13:58:28]  [RadarAPI]: Status: Passed
[13:58:33]  [DeviceId-0] MSS CPU Fault error status Async event recieved(0x3, 0x0,0xFFFFE580, 0x0,0x0, 0x0,0x0, 0xFFFF,0xFF, 0xFF,0xFF, 0xFF)
[13:58:33]  [DeviceId-0] MSS power up done async event received!
[13:58:33]  [RadarAPI]: ar1.PowerOn_mult(1, 0, 1000, 0,0)
[13:58:33]  [RadarAPI]: Status: Passed
[13:58:44]  [RadarAPI]: ar1.DownloadBSSFw_mult(1,"C:\\ti\\mmwave_dfp_02_02_02_01\\firmware\\xwr22xx_metaImage.bin")
[13:58:44]  [RadarAPI]: ar1.DownloadBssFwOvSPI_mult(1, C:\\ti\\mmwave_dfp_02_02_02_01\\firmware\\xwr22xx_metaImage.bin)
[14:26:46]  [RadarAPI]: ar1.SelectChipVersion("AR1243")
[14:26:46]  [RadarAPI]: Status: Passed
[14:26:46]  [RadarAPI]: ar1.SelectChipVersion("AR1243")
[14:26:46]  [RadarAPI]: Status: Passed
[14:26:46]  [RadarAPI]: ar1.deviceVariantSelection("XWR2243")
[14:26:46]  [RadarAPI]: Status: Passed
[14:26:46]  [RadarAPI]: ar1.frequencyBandSelection("77G")
[14:26:46]  [RadarAPI]: ar1.SelectChipVersion("XWR2243")
[14:26:46]  [RadarAPI]: Status: Passed
[14:26:46]  Device Status : XWR2243/ASIL-B/SOP:4/ES:1.0
[14:27:06]  [RadarAPI]: Device Restart failed
[14:27:06]  [RadarAPI]: ar1.RfEnable_mult(1)
[14:27:06]  Status: Failed, Error Type: INVALID INPUT
[14:27:10]  BSS Power Up async event was not received!