Other Parts Discussed in Thread: MMWCAS-RF-EVM, MMWCAS-DSP-EVM, AWR2243
Hi team,
I'd like to inquire how to solve a problem I have.
I bought TIDEP-01012 (MMWCAS-RF-EVM x MMWCAS-DSP-EVM). I am setting up the boards with mmWstudio according to the user's guide of mmWave Studio Cascade.
However, I am in trouble to set up. After I click the RF Power-up button, the error message "BSS Power Up async event was not received!" appeared.
MMWCAS-RF-EVM I use has AWR2243. I use mmWave Studio 3.0.0.14, and xwr22xx_metaImage.bin in mmwave dfp 2.2.2.1.
I already have checked past thread of E2E, however, I have not solved this problem.
Could you please help me?
I put the screenshot of the window with the error message and the full scripts showed in an output window is as below:
GM: Constructor
GM: Wed Sep 02 11:43:55 2020
RSTD.Transmit("/Settings")
[11:43:55]
[11:43:55] ### Running Startup script: "C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\Scripts\Startup.lua" ###
[11:43:55] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[11:43:55] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[11:43:55] Scripter ignored: Attempt to UnBuild() again or before Build.
[11:43:55] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_03_00_00_14\\mmWaveStudio\\Clients\\\\LabClient.dll")
[11:43:55] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[11:43:55] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[11:43:55] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[11:43:55] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[11:43:55] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[11:43:55] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_03_00_00_14\\mmWaveStudio\\RunTime\\SAL.dll")
[11:43:55] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[11:43:55] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[11:43:55] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[11:43:55] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[11:43:55] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[11:43:55] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[11:43:55] RSTD.Transmit("/")
[11:43:55] RSTD.SaveSettings(): Settings saved to "C:\Users\F0004455.S-AE\AppData\Roaming\RSTD\config.xml"
[11:43:55] RSTD.Build()
[11:43:55] RSTD.SaveSettings(): Settings saved to "C:\Users\F0004455.S-AE\AppData\Roaming\RSTD\config.xml"
[11:43:55] RSTD.Transmit("/")
[11:43:55] RSTD.AL_Build()
[11:43:55] RSTD.AL_LoadXml()
[11:43:55] RSTD.Transmit("/")
[11:43:55] RSTD.AL_Init()
[11:43:55] RSTD.Clients_Build()
[11:43:55] GM: Init
[11:43:55] GM: Loaded 'C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\Clients\\LabClient.dll'
[11:43:55] GM: 1 Guest (s) init
[11:43:55] GM: 1 Module(s) init
[11:43:55] GM: 2 Tab (s) init
[11:43:55] RSTD.Client_LoadXml()
[11:43:56] [RadarAPI]: ar1.selectRadarMode(0)
[11:43:56] [RadarAPI]: Status: Passed
[11:43:56] Matlab Runtime Engine is installed
[11:43:56] [RadarAPI]: Starting Matlab Engine..
[11:44:13] [RadarAPI]: Matlab Engine Started!
[11:44:37] [RadarAPI]: ar1.selectCascadeMode(0)
[11:44:37] [RadarAPI]: Status: Passed
[11:44:37] [RadarAPI]: ar1.LoadSettings('C:\Users\F0004455.S-AE\AppData\Roaming\RSTD\ar1gui.ini')
[11:44:38] TESTING = false
[11:44:38] RstdNet: Port 2777: Listening..
[11:44:38]
[11:44:38] ***Script completed successfully.***
[11:48:36] [RadarAPI]: ar1.selectRadarMode(1)
[11:48:36] [RadarAPI]: ar1.selectCascadeMode(1)
[11:48:37] [RadarAPI]: Status: Passed
[11:48:37] [RadarAPI]: Status: Passed
[11:48:38] [RadarAPI]: ar1.SelectCaptureDevice("TDA2XX")
[11:48:38] [RadarAPI]: Status: Passed
[11:48:39] [RadarAPI]: TDAStatusCallback Event Registered
[11:48:39] [RadarAPI]: registerTDAStatusCallback Status: Passed
[11:48:39] [RadarAPI]: ar1.ConnectTDA("192.168.33.180", 5001, 15)
[11:48:39] [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[11:48:39] [RadarAPI]: Device 32 : CAPTURE_RESPONSE_VERSION_INFO Async event recieved() with status 0. TDA Version : REL_VISION_SDK_03_07_01_00 Aug 5 2019 15:04:45[11:48:39] [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[11:48:41] [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[11:48:41] [RadarAPI]: ConnectTDACaptureCard Status: Passed
[11:48:41] TDA Capture Card Status : CONNECTED!
[11:48:57] [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[11:48:57] [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[11:48:58] [RadarAPI]: ar1.FullReset(1)
[11:48:58] [RadarAPI]: Status: Passed
[11:48:58] [RadarAPI]: ar1.SOPControl_mult(1,4)
[11:48:58] [RadarAPI]: Status: Passed
[11:49:10] [DeviceId-0] MSS CPU Fault error status Async event recieved(0x3, 0x0,0xFFFFE580, 0x0,0x0, 0x0,0x0, 0xFFFF,0xFF, 0xFF,0xFF, 0xFF)
[11:49:10] [RadarAPI]: ar1.PowerOn_mult(1, 0, 1000, 0,0)
[11:49:10] [DeviceId-0] MSS power up done async event received!
[11:49:10] [RadarAPI]: Status: Passed
[11:49:32] [RadarAPI]: ar1.DownloadBSSFw_mult(1,"C:\\ti\\mmwave_dfp_02_02_02_01\\firmware\\xwr22xx_metaImage.bin")
[11:49:32] [RadarAPI]: ar1.DownloadBssFwOvSPI_mult(1, C:\\ti\\mmwave_dfp_02_02_02_01\\firmware\\xwr22xx_metaImage.bin)
[11:49:41] [RadarAPI]: ar1.DownloadMSSFw_mult(1, "")
[11:49:53] [RadarAPI]: ar1.SelectChipVersion("AR1243")
[11:49:53] [RadarAPI]: Status: Passed
[11:49:53] [RadarAPI]: ar1.SelectChipVersion("AR1243")
[11:49:53] [RadarAPI]: Status: Passed
[11:49:53] [RadarAPI]: ar1.deviceVariantSelection("XWR2243")
[11:49:53] [RadarAPI]: Status: Passed
[11:49:53] [RadarAPI]: ar1.frequencyBandSelection("77G")
[11:49:54] [RadarAPI]: ar1.SelectChipVersion("XWR2243")
[11:49:54] [RadarAPI]: Status: Passed
[11:49:54] Device Status : XWR2243/ASIL-B/SOP:4/ES:1.0
[11:49:57] [RadarAPI]: Device Restart failed
[11:49:57] [RadarAPI]: ar1.RfEnable_mult(1)
[11:49:57] Status: Failed, Error Type: INVALID INPUT
[11:50:01] BSS Power Up async event was not received!