Hello,
We have a design where the FDC1004 is used for water level sensing with LEVEL and REF electrodes, per respective app note. Everything works at room temp, but has large errors when the device heats up.
When I point hot air (50degC) at the IC, the Clevel and Cref outputs jump up. In the plot below, orange is Clevel and yellow is Cref. As you can see, the capacitance levels increase quite significantly with heat, and as the device cools off, there is some weird quantization in both Clevel and Cref. The quantization jumps are on the order of 0.05pF and completely mess up our measurements, of course. Also, being on the order of 0.05pF, they are much larger than the accuracy stated in electrical specifications.
Any idea what might be going on?
I re-checked the layout and bypass capacitance, no obvious problems there. I am running single acquisitions, so no I2C transitions occur during measurements.