Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843
Hello,
Im reading the data of the AWR1843 with a python-script using the serial port. I saw there is an example for an advanced frame configuration in the doxygen. Im wondering if its possible to read the detected object for each subframe. I saw its possible to see the detected objects for each subframe in the demo visualizer but can I read them with my python script?
What Im trying to do is: I want to detect a smaller object in front of the sensor (about 20 cm) when a big object is behind it. My plan was to use subframes with diffrent CFAR-FOV's. I want to use a subframe with a CFAR range just behind the small object and another subframe to observe a range of 5 m. Is this even the right idea to solve my problem?
Thanks for your help.