This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: MIMO lua scripting template

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR1843BOOST

I there any lua template to use for a MIMO configuration on AWR2243BOOST? Just a 3x4 MIMO setup, TDM or BPM (TDM proffered), no cascading.

Thanks,

Daniel

  • Hello Daniel,

    As such for single chip, we don't have any template but there is an example script with cascade in the mmWave studio package (<download_directory\ti\mmwave_studio_<version>\mmWaveStudio\Scripts\Cascade), so you might want to look at that and get some idea.

    You could also refer to this Application note for a heads up.

    Regards,

    Ishita

  • Ishita,

    The MIMO script in cascade location seems to be compatible with TDA capture card. Which DCA1000 script is the closest to a MIMO configuration?

    Thanks,

    Daniel

  • Hello Daniel,

    As I said, there doesn't exist any specific script for your usecase as such but one thing you can probably do is take reference for the chirp/frame configuration part from the Cascade MIMO script and the DCA1000 configuration commands (also the rest of channel config) from DataCaptureDemo_xWR.lua, 

    Regards,

    Ishita

  • Can you clarify if the Cascade MIMO script (Cascade_Configuration_MIMO.lua) is for a TDM or BPM MIMO?

    Daniel

  • Hello Daniel,

    It is a script for TDM MIMO. You could refer to mmWave_studio_cascade_user_guide.pdf for more details.

    Regards,

    Ishita

  • Thanks.

    Can you also send reference for the APIs in lua scripts, e.g. ar1.ChirpConfig() 

    Looking for the input params.

    Thanks,

    Daniel

  • Hello Daniel,

    - The APIs used in the script can be found in the mmWave Interface Control Document i.e. ICD that is there in mmWave DFP Package. (Although the name is slightly different, but you will be able to locate them using the basic function of that API)

    For eg. for ar1.ChirpConfig(), search for "ChirpConfig" in the ICD.

    -Alternatively, there’s one other feature available for this in mmWave studio called as “help”.

    For the help feature, click on option "lua shell" in the view tab of mmWave Studio and type “help <API>".

    For eg. Type "help ar1.ChirpConfig()" in the lua shell, and you'll get a detailed description of this API. 

    Also, please click "This resolves my issue" button, if your query is answered.

    Thanks & Regards,

    Ishita

  • Ishita,

    The Tx antenna spacing on AWR2243BOOST seems to be \lambda which is twice as that for receiver spacing. In this case the 4 times distance toward the phase configuration of (0, w, 2w, 3w, 4w, 5w, ...) presented in the MIMO Radar document Figure 5, won't be valid. Is this a correct understanding about antenna spacing on the BOOST?

    Daniel

  • Hello Daniel,

    Figure 5 in the MIMO radar document is just a reference example to demonstrate how MIMO radar works and its principle. Figure 5 achieves the same granularity with MIMO concept as what was demonstrated by Figure 4 with less number of antennas.

    Regards,

    Ishita

  • Okay, then what is the phase-antenna mapping for the Rx/Tx config of the current AWR2243Boost board?

  • Hello Daniel,

    As explained in section 3 of the document, the phases can be derived for this usecase.

    The difference here is that if distance between RXs is d, then it will be 2d between TXs, and hence the phase at each RX would be (0,w,2w,3w), (2w,3w,4w,5w) (considering 2TX are transmitting at a time).

    (Please read the document carefully, the part to derive the phase difference is very well explained)

    Regards,

    Ishita

  • Ishita,

    I understand the principal of virtual antenna explained in section 3 of the Radar MIMO document. I found it mismatching with the BOOST board though. Is there any document which explains the phase analysis for this particular use case?

    My question was that an antenna configuration of 12 virtual antenna seems not to be the case for BOOST, as some phases are duplicating. Will the size of angular FFT be 12 as claimed extensively throughout the documents of BOOST? If not, how can the duplicate phases be efficiently addressed in the FFT?

  • Hello Daniel,

    Antenna configuration of AWR2243BOOST is the same as AWR1843BOOST.

    So you can refer the mmwave SDK doxygen document which explain the virtual antenna where there is no overlap in the azimuth virtual antenna.

    file:///C:/ti/mmwave_sdk_03_04_00_03/packages/ti/demo/xwr18xx/mmw/docs/doxygen/html/index.html

    file:///C:/ti/mmwave_sdk_03_04_00_03/packages/ti/demo/xwr18xx/mmw/docs/doxygen/html/coordinate_geometry.png

    Could you refer above path (install mmwave SDK 3.4 first).

     And there you can refer the processing chain documentation for your query.

    Regards,

    Jitendra