Other Parts Discussed in Thread: AWR1443
Hello,
Is it possible to use LUA commands from MATLAB without mmWaveStudio running by using the .NET of mmWaveStudio to open the listening port 2777? Would this cause any future problems? This would allow me to use MATLAB for the entire process instead of usingMMWaveStudio to configure and MATLAB to capture.
If not, is the only option for LVDS capture using AWR1443 and DCA1000 (without mmWaveStudio) to write/modify firmware with the SDK? I thought hardware accelerator function would be something controlled by BSS which users cannot program. But then how does mmWaveStudio allow it to use LVDS?
If anyone can help to clear my thoughts on this, I would appreciate it very much. Thanks, Chase