Dear TI,
Please give some tips for the following phenomenon we observe
When we read the CH0 or CH1 data of LDC1612, the value are sometimes completely
out of range, usually once per hour. The expected values are approximately 52345000
corresponding to a frequency of 7.8MHz with a variation of +/-0.2MHz according to
the position of the metallic object to be detected, knowing that we use an external
clock of 40MHz.
Typical out of range values we read are between 8.5MHz and 20MHz, always higher than the expected frequency.
Before reading a value from the LDC1612, we always check that no error are reported in the STATUS register.
If you have any question or need more information, please let me know.
Best regards.