Hi community member,
I and my customer evaluate 3d_pplcount_demo using IWR6843AoPEVM.
We have questions about the following.
- Which a parameter in the configuration determines the following values?
Azimuth resolution (deg) = 14.5
Elevation resolution (deg) = 58 - . Is "static clutter removal" enable in default config?
I check the "AOP_6m_default.dfg" but there is not parameter of "ClutterRemoval". - According to 3DPeoplecountingDemo_ConfigurationDetails.pdf, static scene processing is enable by "staticRangeAngleCfg".
What difference is static scene enable or disable?
What difference is between static scene and dynamic scene? - 4. What is the parameter"FovCfg"?
There is not an explanation in mmwave SDK user's Guide.
Best regards/.
Cruijff