This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000 Ethernet Communication

Part Number: DCA1000EVM

Hello, 

I would like to connect the DCA1000 board through the ethernet to another PC (not the one which has the mmwave studio tool), the other PC (has the correct static IP) is running a python script that opens a socket with the static IP and the port to capture the raw data through the ethernet from the DCA1000. 

I'm facing the issue that i cannot connect the DCA1000 through the ethernet to any devices (PCs) unless the device runs the mmwave studio.  


I want to configure the DCA1000 using the mmwave studio from PC number one and receive the rawdata from PC number 2 which is the one connected to the ethernet with the DCA1000 

 

Is it possible to do such kind of setup? 

Thanks in advance