Other Parts Discussed in Thread: IWR6843ISK, MMWAVEICBOOST, IWR6843ISK-ODS, DCA1000EVM
Hi
1) We are currently using Ultrasonic sensors on large mulching machines (Think Cat D8 Dozer with large spinning head with teeth instead of a blade) to determine head height above ground but are finding that those sensors simply return the height to the first object returning the ping with any other longer time returns ignored. That first object ideally is the ground, but it could be a weed or a small tree which then causes the head to lift. The saving grace is that the lift/lower hydraulic system is slow and as such by the time the machine has moved forward the next return could be ground before the head has substantially moved.
I was thinking that mmwave radar from the demo's Ive seen could generate returns from all objects in the radars FoV but with some software work I could perhaps track true ground level over things like weeds and small shrubs etc.
I have seen the demo water vs ground but the plot that is shown in the demo, given that you are looking for phase changes associated with water ripples etc doesn't seem to me to be what I would be looking for to determine real ground height.
Is this something that Ti mmwave could be used successfully for?
2) The mulching machine is used to mulch tree stumps that are sticking out of the ground after a tree harvester has cut them off near ground level. Could the mmWave differentiate between ground and wood/stump so that we can see the stumps and use the radar to guide us tracking the tree/stump line? The mulching process generates huge quantities of dust and mulch and as such sight of the stumps can be lost. We use long wave IR Cameras to see the stumps before we can visually see them direct, but even that at time looses sight due to the dust/mulch volumes. I Wonder what effect dust will have on the mmwave radar returns
I would like to get into the eval systems and check this for my self but if it raises flags for you experts then best I avoid the time loss.....
Regards
Andy