This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA460-Q1: Can PGA460 work with 25 kHz

Part Number: PGA460-Q1
Other Parts Discussed in Thread: TUSS4470, PGA460

Hello,

I found some really good transducers with 25kHz frequency. Is it possible to use PGA somehow with this frequency?

Regards,

Gabriel Onzi

  • Hi,

    The PGA460 driver is limited by the clock to the ranges 30-80 kHz and 180-480 kHz. Unfortunately we do not have an AFE that is made to transmit and receive below 30 kHz. The TUSS4470 is able to transmit at 25 kHz because it uses an external clock, although the band pass filter in the receive path has a minimum center frequency setting of 27.48 kHz. Audiowell, Prowave, and Murata are a few good manufacturers that have transducers in the 40-60 kHz range. 

    regards,

    Gabriel