Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
按照指导进行的,可是在用CCS连接目标时总是报错
C674X_0: Error connecting to the target: (Error -275 @ 0x0) The attempt to poll a target device exceeded its timeout limit. The utility or debugger has requested that a target device be repeatedly accessed for a specific data or status value. This has failed because the built-in limit for the maximum number of attempts when polling the JTAG scan-path has been exceeded. (Emulation package 7.0.100.0)
C674X_0: Error connecting to the target: (Error -1146 @ 0x0) Data scanned out of device is corrupt and not valid. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.100.0)
C674X_0: Error connecting to the target: (Error -1146 @ 0x0) Data scanned out of device is corrupt and not valid. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.100.0)
CS_DAP_0: Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 7.0.100.0)
CS_DAP_0: Unable to determine target status after 20 attempts
CS_DAP_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
IcePick_M_0: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 7.0.100.0)
C674X_0: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 7.0.100.0)