Other Parts Discussed in Thread: TDC1000
Hello
I've been using TDC1000-TDC7200EVM boards for a few years now, so I'm pretty familiar with the GUI and the EVM hardware. Since that board is discontinued I purchased a TDC1000-C2000EVM board for our R&D needs.
The problem I'm facing is that after some time or a certain amount of parameter changes in the GUI, the board becomes unresponsive, will stop sending TX waves although it is in continuous mode.
The only way to use it again is to unplug - replug it and restart the GUI. This behaviour seems to aggravate in the sense that the board crashes quicker.
I'm using a win 10 laptop that has been running TDC1000-TDC72000 GUI smoothly for many years, I tried to update the firmware on the board but it already has the latest one.
Do you have any ideas of what could cause this issue ?