Other Parts Discussed in Thread: AWR1642, AWR1843, AWR1642BOOST
Hi,
Below is a screenshot of my Connection Tab in the mmwave studio application. I have not been able to connect either my AWR1642 or AWR1843. The log is also below. It looks like it is successful? But it does not recognize any device. I made sure the COM Port is set up to be the UART port as well.
What are some steps to fix this? I looked in the user guide and there is not much about fixing this issue besides a caution statement about making sure there is 1 device detected and to click the refresh button until it is. I clicked the button a lot and nothing happened.
Thank you!
GM: Constructor
GM: Wed Sep 23 16:54:10 2020
RSTD.Transmit("/Settings")
[16:54:10]
[16:54:10] ### Running Startup script: "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
[16:54:10] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[16:54:10] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[16:54:10] Scripter ignored: Attempt to UnBuild() again or before Build.
[16:54:10] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[16:54:10] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[16:54:10] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[16:54:10] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[16:54:10] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[16:54:10] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[16:54:10] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
[16:54:10] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[16:54:10] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[16:54:10] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[16:54:10] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[16:54:10] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[16:54:10] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[16:54:10] RSTD.Transmit("/")
[16:54:10] RSTD.SaveSettings(): Settings saved to "C:\Users\2019\AppData\Roaming\RSTD\config.xml"
[16:54:10] RSTD.Build()
[16:54:10] RSTD.SaveSettings(): Settings saved to "C:\Users\2019\AppData\Roaming\RSTD\config.xml"
[16:54:10] RSTD.Transmit("/")
[16:54:10] RSTD.AL_Build()
[16:54:10] RSTD.AL_LoadXml()
[16:54:10] RSTD.Transmit("/")
[16:54:10] RSTD.AL_Init()
[16:54:10] RSTD.Clients_Build()
[16:54:10] GM: Init
[16:54:10] GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
[16:54:10] GM: 1 Guest (s) init
[16:54:10] GM: 1 Module(s) init
[16:54:10] GM: 2 Tab (s) init
[16:54:10] RSTD.Client_LoadXml()
[16:54:11] [RadarAPI]: ar1.selectRadarMode(0)
[16:54:11] [RadarAPI]: Status: Passed
[16:54:11] Matlab Runtime Engine is installed
[16:54:11] [RadarAPI]: Starting Matlab Engine..
[16:54:14] [RadarAPI]: Matlab Engine Started!
[16:54:15] [RadarAPI]: ar1.selectCascadeMode(0)
[16:54:15] [RadarAPI]: Status: Passed
[16:54:15] [RadarAPI]: ar1.LoadSettings('C:\Users\2019\AppData\Roaming\RSTD\ar1gui.ini')
[16:54:15] TESTING = false
[16:54:15] RstdNet: Port 2777: Listening..
[16:54:15]
[16:54:15] ***Script completed successfully.***