Other Parts Discussed in Thread: TDC7201, TDC1000
There have been a number of threads on the pulse width of the start and stop signals for the TDC7201.
One of them repeats the specs from the manual that the minimum pulse width is 10 ns.
Another one, which is linked to this question, states that the TDC only checks the rising or falling edge, but not both.
Thus, the corresponding pulse width could be infinite. By that same token, we have a voltage signal with a pulse width of 1 ns. Wouldn't
that pulse width still be acceptable if the device is only checking for the start pulse's rising edge?
Thanks
Keith