Dear TI support,
we would like to detect stationary targets with -35dBsm RCS on a flat surface from max 200m (range resolution is not a limitation).
Based on your mmWaveSensingEstimator tool it should be possible using highly directional antenna (>35dB gain) - could you please confirm this?
Considering that the velocity and the angle of the object (angle can be derived from radar orientation) is not of an interest to us do you think it is possible to use all 4 RX channels together with one antenna to improve the SNR?
Thanks and regards
/Ágoston