Other Parts Discussed in Thread: AWR2243BOOST, , AWR2243, UNIFLASH, AWR1243
Hello,
This is very similar to another post, which did not get solved:
https://e2e.ti.com/support/sensors/f/1023/t/775165?DCA1000EVM-Streaming-LVDS-from-AWR1843-to-DCA1000-without-mmWave-Studio
I also managed to get the data capture demo in mmWave Studio using the AWR2243BOOST connected to a DCA1000EVM.
Now I would like for the AWR2243BOOST with the DCA1000EVM to stream data continuously without being setup by a windows computer running mmWave Studio.
I know there is no linux-support for TI products, but there are many ways this probably can be solved.
It would be perfectly fine if the AWR2243BOOST would run a pre-loaded config created with mmWave Studio.
- Is it possible for the AWR2243BOOST and DCA1000EVM to startup with a pre-loaded config, so that it starts streaming as soon as the devices are powered up?
- Is it possible to (somehow) start both devices via the the ethernet-connector on the DCA1000EVM?
Any other suggestions for solutions is also welcome.