Hello;
I recently starting working with the LDC1101EVM system to measure axial movement over a range of 0-1mm. The target is a titanium cylinder and the sensor coil is a legacy design consisting of 60 coils of wire around the exterior end of a titanium tube. The coil is measuring the interior titanium cylinder as it moves. The cylinder is 8mm in diameter and the coil is 4-10mm in diameter donut. Using the LDC1101-EVM, we have measured the axial movement of the cylinder but we are looking for more response. Questions that I have are:
1) If we decrease the diameter of the sensor under 8mm, would the signal improve?
2) Obviously having a titanium shell between the target and sensor coil will reduce the signal, is there a method to reduce the loss?
3) Would multiple layers of wire improve the signal or just add noise?
Thanks for any help.
Scott