Hello I have some question about IWR6843ISK
1)We know IWR6843ISK support to extend maximum velocity to 2x, we want to know what principle is used. And does it needs to operate in a specific mode (e.g.: MIMO).
2)Known radar cube size is 768kB in IWR6843ISK, we want to improve velocity resolution. Now we encounter some terrible by increase chirp numbers(M) in a frame.
Our goal is to achieve max range is 90m, range resolution 40cm, max velocity 90km/hr, and velocity resolution 1km/hr at the same time.
Below is the cfg. file setting we want to tune:
profileCfg 0 60 22 7 28 0 0 20 1 256 12500 0 0 48
frameCfg 0 1 96 0 50 1 0
we calculate N=256 and M=96 will not exceed 768kB, but now we only can set M=80, which can let radar work.
The error report return by MATLAB tm_visualizer is:
The original M is 64, we also tune M value within 64 to 80 but most of the value can not let the radar work. The error report is the same as the above.
Looking forward to your reply.