Hello TI team,
I am looking at the overhead people counting lab of the latest version 4.4.1. I was curious if I could turn off the tracking engine completely (let's say the tracking and classification is done externally).
1. How do I do it correctly? I tried to use "trackingCfg 0 2 800 20 37 33 120" - in this case it seems like something goes wrong and no data is coming, but maybe I am doing something wrong? I also tried to use "trackingCfg 1 2 1 20 37 33 120" - simply to restrict the number of acceptable points, it all works and no tracking is being performed, but I wonder if the tracking engine is still being allocated?
2. Assuming the tracking engine is not running through the Firmware, does it mean certain resources are now free (e.g., memory and processing power) and I could maybe tune the chirp config in a way so that it requires more memory/processing time; or perform some other functions? Is there any way to calculate how much of the resources is freed if the tracking engine is not used?
Best regards,
Victoria