This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Es3 IWR1443 flashing

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: UNIFLASH, CCSTUDIO

Hi

I have iwr1443boost ES3 version. I want to use the demo visualiser to see the live plots. I use SDK 2.1 to flash the firmware which is ..\ti\utils\ccsdebug\xwr14xx_ccsdebug,bin file. I got the message in Uniflash that the flashing was success. For flashing I used SOP 101. Then I removed jumpers from SOP2. When I tried to connect using demo visualiser 2.1, it just shows hardware connected. No messages on the console and no plots. I wonder where am I going wrong.

I think  it  is because of the bin file I chose to flash the module.

Would you be able to help me out.

Many Thanks,

 

  • Hi Sruthy

    You will want to flash the device, using the same flashing procedure, but with the demo binary. You can either compile this binary by downloading the CCSTUDIO Projectspec files from the lab and building the executable using the procedure in the Lab User Guide.

    Or more simply you can download the prebuilt binary included in the SDK at the following location:

    C:\ti\mmwave_sdk_02_01_00_04\packages\ti\demo\xwr14xx\mmw\xwr14xx_mmw_demo.bin

    Regards,

    AG