I'm ongoing develop linear polarization resistance sensor. Using LMP91000 as AFE and read by ADC 16 bit.
Measured total resiatance on water fluid. An result in corrosion rate.
How to calibrate the lmp91000 AFE?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm ongoing develop linear polarization resistance sensor. Using LMP91000 as AFE and read by ADC 16 bit.
Measured total resiatance on water fluid. An result in corrosion rate.
How to calibrate the lmp91000 AFE?
Dear Hendry -
Welcome to the E2E Forum and thanks for posting!
From what I could gather on this topic, this is a non-destructive method of determining the corrosion rates of metals that basically involves the sensor being excited and the potentiostat sweeping the metal under examination
This seemed like a good reference to share: https://www.gamry.com/application-notes/corrosion-coatings/basics-of-electrochemical-corrosion-measurements/
I think once you get a reference device to compare what you are developing to and go through the math like what i can see in the link provided, it might become clear what the settings should be on the LMP91000 and what calibrations you may need to do to your system (not the LMP91000 itself).
Hi Josh,
I'm using LMP for reading oxygen in liquid(water) by converting from current "uA" reading.
Currently using 3 electrode , intrusive to the pipe. Using flange and access fittings.
The last calibration method that used are using 2 resistor 60 ohm, 1 connected to CE and RE, 1 connected to WE and RE.
Is that correct method? Or i must calibrate using conductivity liquid, by dipped the 3 electrode to it?
Dear Hendry -
I would recommend using a reference sensor and the EVM, in the physical configuration you intend. Perhaps a 2 lead cell configuration as is done with O2 sensors, start with a configuration from the sensor database in the GUI, and modify until you get to reasonable values first, then check over temperature, then go look for things you may have to tweak or "calibrate" - for example, the cable connection between the sensor and the AFE is usually something that is needed to be attended to when designing low power measurement systems.
Hi Josh,
Thank You for information,
this is sensor that i mean.
and what type of reference sensor? something like this below?
BR
Hendry
Hendry -
I meant that you would create a reference system, with known good working components, as you develop your sensor.