I have the 6843AOPEVM
The instructions for the people counting demo clearly specify that the demo works with this model, it shows pictures of the model and mentions it explicitly
I followed the instructions bu no joy
I successfully flashed the pre-compiled bin file.. but...
First of all, I installed the demo visualizer on 2 separate windows 10 machines, 1 laptop, 1 desktop, both times it will not let me load a config file. Clicking "select config" does nothing at all.
So I went back to my linux box. Serial terminals seems to work.
I can set the config setting at the prompt on the 115200 baud port, everything there is working fine
but the data port is garbage, I cant find the header magic word to identify the packet header.. looking at the data my instinct tells me incorrect baud rate,but nothing works, tried all baud rates, garbage data no matter what.
The unit is clearly functioning, i can see it sending data when it detects people and stop sending when there are no people in range.
I found old posts suggesting that I need to modify the source because it is not compatible with AOP, but I also found lines in the source that clearly reference the AOP. Moreover if this is the case why is there no mention of it in the documentation. the documentation clearly says this model works but make no mention of any special steps required for this model.
Do I need to recompile the bin file? do i need to edit the source? What is going on?
I can live with just access to the raw output data alone, but it would be cool if the windows demo visualizer also worked, so does anyone know whats going on there?
I can enter com pots and click connect.. but it always connects, even if I put com ports in incorrectly.
clicking "select config" does absolutely nothing.
and if I edit the sensor position parameters and hit enter then "connected" changes to "unable to connect"
but my priority is just getting good data. visualizer secondary and not necessary.