Other Parts Discussed in Thread: AWR2243
Hi,
When I detect something with the MIMO configuration lua file and the capture.lua, the calculus made in mmWave Studio 03.00.00.07 are 3GHz of Bandwidth. When I check the tab of "calculated parameters" in PostProc, it says that the start frequency is 77GHz and the stop Frequency is 77.5 GHz (0.5 GHZ of bandwidth per chirp, instead of the 3 GHz which were set)
Could you please tell me why Matlab calculates 1/6 the bandwidth? Which one is correct, Matlab's or mmWave Studio calculation?
Best regards,