Hello TI team,
I've been looking at the Overhead 3D people counting lab, and noticed one of its requirements is the calibration procedure in order to obtain compRangeBiasAndRxChanPhase coefficients.
I also noticed that the default values of those coefficients are "0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0", while the "3D point cloud data" lab has default coefficients as "0 -1 0 1 0 1 0 -1 0 -1 0 1 0 1 0 -1 0 -1 0 1 0 1 0 -1 0" (some of them are negative, and as I understand it is so that to take into account rotations of some of the antennas).
1. So how come the default coefficients of the compRangeBiasAndRxChanPhase parameter are different for the two firmware? When I tried to use the default values with negative signs, the point cloud coordinates got inverted along X axis, it seemed. Could it be the "overhead people counting" firmware negates the necessary coefficients on the firmware level?
I had also performed a calibration procedure with my sensor and obtain the calibrated values so that to use them within the "overhead people counting" lab.
2. Is there any visual difference that is made by using the calibrated values? Is it something that I'm expected to see? How does that difference help the "overhead people counting" lab to be more precise? I'm just trying to understand if the calibration procedure is critical and whether it has a great impact on the performance of the "overhead people counting" lab.
Thank you.
Best regards,
Victoria