Hi,
My customer use the OOB demo to calibrate their board which antenna is similar to ISK, got the phase factor as input to compensate the channel phase difference. Then found one strange issue that there are great improvement near the bore sight, we can see more points number detected, while at the edge angle such as +-30/45degree, the detection points number decrease a lot.
My question is what is the impact of the current calibration in OOB in full FOV, can it improve all the detection performance in full FOV?
Any comments is welcome, it is a little bit urgent, look forward to your reply, thanks.
Andy