This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Setting for over 200m

Part Number: AWR1843

Hi Expert!

Q1: Is there any problem with the RF characteristics on AWR1843 even if the setting is over 200m?

Q2: Please let me know if there is a parameter that can set 230m with a distance resolution of about 50cm.

      It is a problem because the resolution becomes rough at a long distance.

      If there is something that can be set with CLI commands the I would like to try it.

 

Thanks and Best regards,

Hata.