This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: IWR6843AOP(ES2.0): RadarCubeCompression(HWA1.1)

Part Number: IWR6843AOP
Other Parts Discussed in Thread: IWR6843

Hello,

IWR6843AOP(ES2.0): RadarCubeCompression(HWA1.1)

after:

swra663(_MemCompressionRadarCube).pdf:

This paper also introduces the TI Memory Compression/Decompression Engine, a hardware module that
is newly added to the TI millimeter wave radar solutions. It is included in the IWR6843 and other upcoming
radar devices that contains hardware accelerator (HWA) version 1.1 or above.

swru522e.pdf:
                        HWAV1.0                                    HWAv1.05                      HWAV1.1
Device        IWR1443ES1.0,ES2.0,ES3.0    IWR6843    ES1.0        IWR6843 ES2.0

we should have the needed HWA (HW support).

Our RadarCube is 75% of L3-RAM

Atm RAM is the Limiting Factor for our Applikation...

Any help in for of Hwa Drivers, DemonstationUsageCode, even HW-RegisterDefinitions/Desription is good to us,
it must not be a compile and okay version.
From HWA manuel we even dont understand which Register would have to be used..

kind regards