Hi,
I understand that the IWR1642 does not support CW, but the customer wants to measure CW mode with a spectrum analyzer. Is this test possible with the SDK1.1 capture demo?
* Due to their product specifications, "mmwave studio" cannot be used because there is no 60pin connector on the customer board.
UART settings are as follows, but they are not output. but it does not output.
Are the following settings correct?
------------------------------------------------------------------------------------------------
C:\ti\mmwave_sdk_01_01_00_02\packages\ti\demo\xwr16xx\capture\xwr16xx_capture_demo.bin
flushCfg
dfeDataOutputMode 2
channelCfg 2 1 0
adcCfg 2 2
adcbufCfg 0 0 1 1
lowPower 0 0
contModeCfg 77 0 0 6000 0 0 30 1 1024
setHSI LVDS ADC disable
sensorStart
---------------------------------------------------------------------------
Best regards,
Hiroshi