Hi, we have a customer with a concern as below.
I would like to have a dual mode chirp.
The first chirp is for the object location, and this is a standard chirp and it works quite well. Second chirp has following features
1) There are three transmitters to get maximum range and angular resolution. The mode is sequential.
2) the chirp time should be long, e.g. 10 ms. Or we can have several short chirps and average the data of these. This is to get as good SNR as possible.
3) the repeating time is 200 ms,
4) We want to get complex amplitude data, range and angle of arrival. Or we can use the angular data of the first chirp to get complex amlitude data from the object, that we know the location on the basis of the first chirp.
Problem is that I don't know how to generate such a chirp. Is the MMWAVE DFP right tool for this? It seems difficult to get it running.
Appreciate your help.
regards,
roland