This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mmWave studio chirp and frame settings



Hello,

In mmWave Studio (V2.1), Sensor Configuration tab, Frame settings:

When the duty cycle is less than 100%, does the off time comes after each chirp in the frame? or does it come after the whole no of frames?

For example, in one frame if the No of chirp loops is 5 and the duty Cycle is 50%

Does it go like: chirp   off   chirp   off   chirp   off   chirp   off   chirp   off

Or: chirp chirp chirp chirp chirp off 

Thank you.