Hello,
I have some questions about clutter removal function of AWR1642.
I understand calculation procedure of clutter removal.
(The mean value of the input samples to the 2D-FFT is subtracted from the samples.)
Although removal static clutter is enaled, target that have zero doppler index is detected sometimes.
Please see the picture below.
In our office, when AWR1642 is not moving (AWR1642 is put on my desk), there is no detected object, because there is no moving object around AWR1642.
But once I move AWR1642 , since there are relatively moving objects, some detected objects appear, and
in range profile for zero doppler plot, there is one detected object.
(I think it is spectral leakage of FFT.)
Do you have any ideas why target at zero doppler is detected in spite of enabled clutter removal?
SDK: SDK2.1
C:\ti\mmwave_sdk_02_01_00_04\packages\ti\demo\xwr16xx\mmw\xwr16xx_mmw_demo.bin
mmWave demo visualizer: 3.1.0