This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000

Part Number: DCA1000EVM


Dear engineer:
        Hello, when running mmWaveStudio 2.0.0.1, an error like "Application already running. Only one instance of this application is allowed" appears. But the running software was not found in the task manager. It is installed in the ti folder of the C drive, but after the installation, the corresponding software cannot be found in the control panel, the uninstall operation cannot be performed, and the software cannot be started. What is the reason for this and how to solve this problem? Looking forward to your reply.Thank you!

  • Hello User,

    To uninstall mmWave Studio, delete the following: 

    1. RSTD folder; located here C:\Users\<USERNAME>\AppData\Roaming\RSTD
    2. mmwave_studio_02_00_00_01 folder; located here <download directory>\ti\mmwave_studio_02_00_00_01

    Re-install following the instructions in the mmWave studio user’s guide in section 2.1 (Installation).

    Also, you can just make sure if some exe or some other mmWave studio file is not lingering by going to the "Services" Tab in the Task Manager. If you see any mmWave studio file there, just kill that and try again. If that doesn't work then re-install studio.

    Regards,

    Ishita