This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Can the Ramp End Time shorter than default one for People Count Demo

Part Number: IWR6843AOP

Hi community member,

My customer have a question about the chirp for people count demo(ITB4.4.1).
They consider that a ramp end time is shorter than a default one.
Because they need to adjust to 10% of on-time duty due to Japanese radio regulation.

How short can the ramp end time of People Count Demo?
Best regards.
Cruijff

  • Hello

    With the updated Chipr what does the  new sensing parameter come out to be. That should be computed.

    Based on that the demo should be tuned to meet the application needs.

    Can you please help us understand the regulation needs that have to be met?

    Thank you,

    Vaibhav