What are the ramifications of using a 1 kOhm pull up on a 5V line driving the TMP275AIDR? The data sheet states 3 mA maximum, but the design is working with the 1 kOhm pullup (5mA) in the lab. The I2C bus has 8 different devices on it and the original 2.1 kOhm pull up was not meeting the 300 nS rise time in all cases so we are considering a 1 kOhm part instead.