We want to test the performance of AWR1642BOOST-ODS in detecting distant obstacles. As the description of user guide, the range setting of Lab demo is 0 to 2 meters.
May I use which configuration parameter to modify the setting range? Can you give me an example?
Default configuration setting for ODS demo:
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 0 1 1
profileCfg 0 77 7 7 58.0 0 0 67.978 1 256 5020 0 0 36
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 32 0 100 1 0
lowPower 0 1
guiMonitor 1 1 0 0
cfarCfg 1 4 12 4 2 8 2 350 30 2 0 5 20
dbscanCfg 4 4 13 20 3 256
sensorStart
Thanks