This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AC Power Monitor

Other Parts Discussed in Thread: EVM430-I2040S

Hello,

I have an application to measure current (max up to 15A) and voltage of an input AC source . The input AC voltage can be from 2 different sources and is expected to be within 115-240 VAC, with one source being 60Hz and the other is 400Hz.

I had seen the evaluation board EVM430-I2040S for this application but it seems like this is an obsolete part.

Do you have any ideas or components that I can use for my application.