Part Number: MMWCAS-DSP-EVM
Other Parts Discussed in Thread: AWR2243, MMWCAS-RF-EVM, AWR1243, TDA2
Hello!
I'm working with the MMWCAS-DSP-EVM paired with a MMWCAS-RF-EVM using AWR2243 radar devices. I have successfully run the mmWaveLink_Cascade_Example from MMWAVE-DFP-2G version 2.2.2.1. I would like to write my own application which continuously streams ADC data from the AWR2243 devices to the host computer over ethernet rather than logging it to the SSD on the DSP-EVM.
I think I have a good idea of how to do this on the host computer, but I would also need to modify the code running on the DSP-EVM and I can't find any information on how to do that. Is there any documentation on how to write and build applications to run on the DSP-EVM? Also, it would be very helpful if I could refer to the source code for the application that runs on the DSP-EVM and communicates with the mmWaveLink_Cascade_Example running on the host computer. The binary for that application came pre-installed on the DSP-EVM's micro-SD card, but I haven't been able to locate the source code. Could you tell me where to find that source code?
Thank you so much for your help!