Hi,
In the datasheet for IWR6843 it seems to be specified what the maximum frequency/us change is (266MHz/us).
I have 3 questions:
1. What would be the slowest we could set it to be?
2. Also are there limitations on frequency bands of use for slow rates? Ive seen in some posts that its best to avoid 62.1 GHz in general. Is that still the case?
3. what documentation and/or tool is best to use to investigate different type of chirp, frequency setups for the IWR6843. thanks.