This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1614: Metal detection application

Part Number: LDC1614

Hello Team,

My Customer is working with an application, which will be installed under a vehicle body to detect the vehicle pass over road lines covered by metal sheets. They wanted to confirm if the LDC1614 and the use of conductive sensing technology are suitable for it. Do we have other solutions we can offer?

Detection is not required to be fast. Only required to be face to face with the metal sheets and the range is 40 cm.

Regards,

-Renan