Hi support team.
My customer is considering TO-92 package of DRV5032.
So they have three questions.
Q1:
They want to fix the space surrounded by the red square in the figure below. What kind of method is there?
Is there only a way to use spacers?
Q2 : Please tell me the size of the width of the protrusion of the lead of the TO-92 package. (Including tolerances)
Is it possible to stop using the protrusion of the lead with the hole size (φ0.75) shown in figure of the land pattern example?
Q3 :
Does it affect the detection accuracy when implemented as shown in the figure below? Are there any other issues?
I would appreciate it if you could reply.
Best regards,
Higa