This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how an accelerometer behave in acceleration and deceleration

Other Parts Discussed in Thread: DRV-ACC16-EVM

Greetings,

                 Please explain me how an accelerometer behave in deceleration (is it gives +ve or _ve values) and how it behaves in acceleration(is it gives +ve or _ve values).

                 consider  object moving in single axis only.

Thank you

  • Hi, Nakka,

    Welcome to E2E and thank you for your interest in our products!

    I strongly recommend to take a look at one of our accelerometers solutions for three-axis acceleration measurements.

    https://www.ti.com/lit/ug/slou402/slou402.pdf

    The EVM converts the acceleration from mechanical movement to mV at a rate of 57 mVpeak per gpeak. This means that every 57 millivolts of peak voltage equals 1 g of peak acceleration and 114 mVpeak equals 2 g’s of peak acceleration. In addition, as mentioned in section 3, there's a DC offset at 1.5V. If the acceleration is positive, you should see a level above 1.5V. When the acceleration decreases, the voltage level is below 1.5V.

    Please let me know if you have additional questions or comments.

    Best regards,
    Luis Fernando Rodríguez S.

  • Hi,
       Thank you for your answer,
                                                             Let us consider accelerometer is firmly fixed to a vehicle in a way that Z axis pointing to downwards, X axis pointing to vehicle forward direction and y Axis is perpendicular to the vehicle.Here X and Y axis are independent of Gravity(if the mounted surface is Ideally flat) and dependent on movement of the vehicle(Jerks).

                           I am moving in X direction , I initially started, that means Accelerated in X direction, then what is the behaviour of accelerometer in X direction only (Desired output: It should give +ve values). Please check it once

                         Now after acceleration , i am moving constant speed that means no acceleration ,Now What is the behavior of accelerometer  in X direction only (Desired Output: It should gives me output approx Zero). Please check it once.

                         At last  I want to stop the vehicle by applying the brakes , then vehicle slows down(rate of change of velocity is negative) means deceleration, At this point what is the behavior of the accelerometer in X direction only (Desired output: It should gives me Negative values). Please check it once.

    Please check these characteristics once and give me your detailed explanation.

    Thanks in Advance.

  • Hi, Nakka,

    Usually, we don't support this kind of questions in this forum since there are no IC accelerometers in this product line. Actually, I think there are no accelerometers in any product line of TI (if I'm not wrong).

    The only solution we have as an accelerometer is the DRV-ACC16-EVM, but it doesn't use a TI IC solution, so we cannot provide deeper details besides the ones described in the User's Guide. In addition, this is an accelerometer designed for low power actuators, so we cannot guarantee a behavior on an automotive solution.

    Do you already have an IC accelerometer in mind? Have you contacted the IC manufacturer for details?

    Thank you.

    Best regards,
    Luis Fernando Rodríguez S.