This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: lose data when capturing raw data

Genius 13655 points
Part Number: AWR1243


Hello,

Customer met many warnings when using AWR1234 to capture data. It captured  75216KB instead of 80000KB.

BSS and MSS:

C:\ti\rf_eval_firmware\radarss\xwr12xx_xwr14xx_radarss_ES3.0.bin

C:\ti\rf_eval_firmware\masterss\xwr12xx_xwr14xx_masterss_ES3.0.bin

The host log is below:

[10:00:05]
[10:00:08] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:00:08] [RadarAPI]: Sending start_record command to DCA1000
[10:00:10] [RadarAPI]: ar1.StartFrame()
[10:00:10] [RadarAPI]: Status: Passed
[10:00:10] Frame start async event received!
[10:00:11] Time Unit report async event received!
[10:00:11] Time Unit report async event received!
[10:00:11] Time Unit report async event received!
[10:00:11] Time Unit report async event received!
[10:00:11] Time Unit report async event received!
[10:00:11] Time Unit report async event received!
[10:00:11] Time Unit report async event received!
[10:00:11] MSS RF Error status Async event recieved(0x1)
[10:00:11] [RadarAPI]: Frame Ended
[10:00:14] [RadarAPI]:
[10:00:14] Start Record command : Success
[10:00:14]
[10:00:14] Record is completed
[10:00:14]
[10:00:14] Record stop is done successfully
[10:00:14] BSS CPU Fault error status Async event recieved(0x3)
[10:00:14] [RadarAPI]:
[10:00:14] Reserved(0x0)
[10:00:14] LineNum(0x2FC)
[10:00:14] FaultLR(0x26EC8)
[10:00:14] FaultPrevLR(0x0)
[10:00:14] FaultSPSR(0x19F)
[10:00:14] FaultSP(0x800FBB0)
[10:00:14] FaultCauseAddress(0x0)
[10:00:14] FaultErrorStatus(0xFFFF)
[10:00:14] FaultErrorSourced(0xFF)
[10:00:14] FaultAXIErrorType(0xFF)
[10:00:14] FaultAccessType(0xFF)
[10:00:14] FaultRecoveryType(0xFF)
[10:00:14] Reserved2(0x0)
[10:00:14] BSS ESM Group1 Fault error status Async event recieved(0x0)
[10:00:14] BSS ESM Group2 Fault error status Async event recieved(0x0)
[10:00:14] Analog fault Async event recieved(0x0)
[10:00:14] Reserved(0x0)
[10:00:14] Reserved2(0x0)
[10:00:14] FaultSig(0x0)
[10:00:14] Reserved3(0x0)
[10:09:33] [RadarAPI]: ar1.StopFrame()
[10:09:37] Status: Failed, Error Type: RESP TIMEOUT

Thanks.
Rgds
Shine