This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843: Frequency range

Part Number: AWR6843


Hi,

the 60 GHz radar chips are specified for 60 to 64 GHz.

It would be useful for us to use a slightly larger range for antenna testing (not used in production units). Is it possible to set up a chirp e.g. from 59 to 60 GHz? 

If not, is it a hardware or software limitation?

Sebastian