Other Parts Discussed in Thread: TDC7200, TDC7201, , TDC7200EVM
A few users of my Rasperry Pi Python 3 driver for the TDC7201 are wanting to use it on the TDC7200 instead. Is there a document describing just the differences between the two chips and EVMs? I don't own a 7200 EVM so I can't really test it, but it doesn't seem like it would take much extra effort.
The driver can be installed from pypi with "python3 -m pip install tdc7201", and the source code is on GitHub. The latest version is 0.10.0, which is late beta and has a very close to complete feature set for side 1 use. It's also very stable; my current test code performs about 2650 measurements/second and can run for weeks unattended.