Other Parts Discussed in Thread: AWR1642
. I have gone through the Demo Visualizer manual and it is not clear to me where are the zero (0) references for the Azimuth and Range data in the scatter plot. I am assuming that the reference for the Range (Y axis) is the minimum of all distances to the object and the azimuth (X axis) is the mid point between TX and RX Antennas per the Figure wx of document Millimeter Wave (mmw) for XWR16xx .
I am working in a static environment, meaning my objects stationary, but my set-up introduces clutter, is there a way I could eliminate this clutter though calibration. Presently the clutter calibration takes the real stationary object as clutter.
With regards to elevation points in the scenery, for the AWR1642, how are these recorded; are they part of the X and Y coordinates or just one axis for, example the range (Y) axis.